cancel
Showing results for 
Search instead for 
Did you mean: 

How can I use the different ports of the MCU for the schematic on EAGLE software?

Vivek Karna
Associate II

I am designing a schematic for my project which uses the STM32F779BI microcontroller. I am using the LQF208 package of the microcontroller. The symbol of the microcontroller is available at different websites but during the schematic design of the microcontroller, all the 208 pins of the microcontroller are present, for that to make the connections for the different pins all the circuit is looking messy. I want that if the symbol of the micrcontroller is available with different blocks or ports, like PORTA, PORTB etc. There would be ease for making the connections if every port are available for the connection.

2 REPLIES 2
JoniS
Senior

You could make such symbol yourself, that's how you get what you want.​

oeliks
Senior

Try to edit symbol, and just move pins. Some lbr cant be edited some can. And You dont have to rename all 208 pins then =) worth to try.​