cancel
Showing results for 
Search instead for 
Did you mean: 

7 COM LCD on STM32WB55Rx

BVern
Associate

Hello,

The datasheet for the STM32WB55 says that the STM32WB55Rx (the VFQFPN68 version) has 4x28 LCD capability.

The same datasheet lists LCD_COM4, LCD_COM5 and LCD_COM6 as alternate functions for pins PC10, PC11 and PC12 which correspond to pins 58, 59 and 60 on the VFQFPN68 package. Are these alternate functions actually usable on the STM32WB55Rx which would mean that I'm able to drive a 7x25 LCD?

Sincerely,

Ben Vernier

0 REPLIES 0