cancel
Showing results for 
Search instead for 
Did you mean: 

I want my st25dv64k to communicate with stm32 mcu using i2c. Is it necessary to power st25dv64k with 3.3v or will Energy Harvesting able to power i2c communication in presence of a NFC Mobile.

RGeorge
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
S.Ma
Principal

Can't answer generic question. Power consumption of STM32H7 is a bit different than STM32L0

If it is a must, you need to do a power budget homework and also prepare the MCU S/W for all the low power modes and also the detection of a failing power supply, size properly the decoupling caps etc...

View solution in original post

1 REPLY 1
S.Ma
Principal

Can't answer generic question. Power consumption of STM32H7 is a bit different than STM32L0

If it is a must, you need to do a power budget homework and also prepare the MCU S/W for all the low power modes and also the detection of a failing power supply, size properly the decoupling caps etc...