cancel
Showing results for 
Search instead for 
Did you mean: 

MX 5.4.0 Bug: <Error generating MDK project file>

Yzy.1
Associate

I downloaded and installed stm32cubemx version 5.4,and the default installation configuration is maintained.When I tried to generate an MDK project, I reported an error.

But it can be used normally after uninstalling and installing version 5.3.

I don't know why?I have tried to uninstall and then reinstall, or check if there is a Chinese path and other methods, which are not available for normal use.

Help me...

I use the win10 64 bit system.

java version "1.8.0_231"

Java(TM) SE Runtime Environment (build 1.8.0_231-b11)

Java HotSpot(TM) Client VM (build 25.231-b11, mixed mode, sharing)

0690X00000BuxR7QAJ.jpg0690X00000BuxR2QAJ.jpg0690X00000BuxRCQAZ.jpg0690X00000BuxRHQAZ.jpg

0690X00000BuxRMQAZ.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Yzy.1
Associate

Now it's solved. It should be a Java environment configuration problem. I need to uninstall JRE again and install it again. Sorry...

View solution in original post

2 REPLIES 2
Yzy.1
Associate

Now it's solved. It should be a Java environment configuration problem. I need to uninstall JRE again and install it again. Sorry...

TTOPA
Associate

Uninstall the java program installed on the computer and install the current version again. It will be fine.