cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-NFC05A1 GUI Tools

JSu.1
Associate II

Hello,

Is any PC GUI tools with X-NUCLEO-NFC05A1 for function estimation easy?

X-NUCLEO-NFC05A1 can be adapter with NUCLEO-F401RE MCU board, but it has no PC GUI tools to work with NFC function estimation as 3911B-Discovery board.

I only saw the firmware driver available?

please kindly advice.

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

the structure folder is described in the User Manual UM2253. For NUCLEO-F401RE , the binaries for the applications are located in: STM32CubeExpansion_NFC5_V2.0.0\Projects\STM32F401RE-Nucleo\Applications\PollingTagDetect\Binary

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi,

X-NUCLEO-NFC05A1 can be used with X-CUBE-NFC5 software expansion package. This package provides 2 turnkey sample applications: the first application detect tags and displays tag UID on the serial com port; the second application reads and display an NDEF message on the serial com port. On PC side, only a serial com terminal is needed to display the informations sent by the applications. No GUI is needed for those sample applications.

X-NUCLEO-NFC05A1 can be used to easlily prototype an application by reusing the sample applications provided by ST.

Feel free to provide more information about your use case and specific needs.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hello, Sir
As you mention 2 turnkey samples application, where folder they located in X-CUBE-NFC5 firmware after uncompressed .zip?
[cid:image001.png@01D5B728.CBDBC450]
Thank you.
Jerry
Brian TIDAL
ST Employee

Hi,

the structure folder is described in the User Manual UM2253. For NUCLEO-F401RE , the binaries for the applications are located in: STM32CubeExpansion_NFC5_V2.0.0\Projects\STM32F401RE-Nucleo\Applications\PollingTagDetect\Binary

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.