cancel
Showing results for 
Search instead for 
Did you mean: 

Azure FOTA on STM32L475

Raju1
Associate

Dear friends,

I am facing one issue with FOTA on Azure platform.We are trying with evaluation kit (B-L475-IOT01A2)The errors seen are

Download FOTA from: HostName=[stm32blob.blob.core.windows.net] Type=[Secure] port=[443] File=[/firmware-nucleo/Azure_Sns_DM.bin]

Ok reported State [3]: Downloading

-->DeviceTwin CallBack [3]: Status_code = 204

Ok io_interface_description

Ok xio_create

Ok xio_setoption

13-11-2019 15:55:58.183 [RX] - ***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_tls.c (3518): bad message length

***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_tls.c (3729): mbedtls_ssl_read_record_layer() returned -29184 (-0x7200)

***\en.fp-cld-azure1\STM32CubeFunctionPack_AZURE1_V3.3.2\Middlewares\Third_Parties\mbedTLS\library\ssl_cli.c (1454): mbedtls_ssl_read_record() returned -29184 (-0x7200)

onOpenCompleteFOTA

Ok xio_open

Err: xio_send

Kindly help me resolve this issue.

Thanks,

Raju

0 REPLIES 0