cancel
Showing results for 
Search instead for 
Did you mean: 

Why max Voltage 50V on IHM03A1 development board?

TYilm.2423
Associate

The recommended voltage range is 85 volts which is also the same as the recommended voltage for the POWERSTEP01 device.

Why max Voltage 50V on IHM03A1 development board?

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @dungeonlords789​,

the STM32 Nucleo Expansion boards for safety reason is limited to max 50 V of power supply.

View solution in original post

3 REPLIES 3
dungeonlords789
Senior III

The same question

@Cristiana SCARAMEL​

Uwe Bonnes
Principal II

Maybe security issues? Higher voltages need protection from touching.

Hi @dungeonlords789​,

the STM32 Nucleo Expansion boards for safety reason is limited to max 50 V of power supply.