cancel
Showing results for 
Search instead for 
Did you mean: 

Project copy/paste doesn't work

PHryn
Associate III

Hi all,

Afer copy/paste of project cubemx .ioc file name is not updated accordingly and cannot be opened.

Manual updating name of .ioc file is fixing this issue.

Regards,

Pawel

1 ACCEPTED SOLUTION

Accepted Solutions

Ok, so you copy through the Project Explorer inside CubeIDE?

I see that it doesn't change name of ioc and content of ioc points to old project as well.

I'll write a ticket for it!

View solution in original post

5 REPLIES 5
Markus GIRDLAND
ST Employee

Just so I understand it correctly:

If you have the project:

C:/workspace/myProject

Then you copy it in Windows it will rename it to:

C:/workspace/myProject - Copy

But the .ioc file is still pointing towards C:/workspace/myProject and any change made will be made towards that project when you generate code etc.

And that's what this issue is about, right?

PHryn
Associate III

Im using Ubuntu, but copy/past it is basic Eclipse function.

To reproduce click in CubeIDE right mouse button over the project and then Copy and again Past.

Project is copied but ioc file stli is pointing to previous project name and when you try to open it it says:

Invalid Input: Must be project's active .ioc file.

Project's 'App_test001' active one is 'App_test001.ioc' file

Then ioc file in project has name App_test000.ioc.

During project copying ioc file should be renamed inline with project.

Regards,

Pawel

Ok, so you copy through the Project Explorer inside CubeIDE?

I see that it doesn't change name of ioc and content of ioc points to old project as well.

I'll write a ticket for it!

PHryn
Associate III

Thank you Markus,

My other wish is option to save SWO output to file or some other possibility to have acces to SWO.

https://community.st.com/s/question/0D50X0000BcR3uwSQC/save-swo-to-file

Why?

Segger support for stm32g4 is shaky and I moved to smt32cubeIDE but here I'm lack RTT tools.

At the moment I try to write RTT using openOCD but here another problem is that support for STlink3 is not great (https://sourceforge.net/p/openocd/tickets/259/)

Regards,

Pawel

Regards,

Pawel

Those signatures seem to do more harm than help...