cancel
Showing results for 
Search instead for 
Did you mean: 

Can I remove the on board display and use the Newhaven display with this development board?

Ehill.16
Senior

Can I remove the on board display and use the Newhaven display with this development board?

3 REPLIES 3
S.Ma
Principal

How about this one?

"Can I remove the on board display and use the Newhaven display with this development board?"

What development board? Provide context, your post is far too vague and non-specific.

https://community.st.com/s/question/0D50X0000BfuZ3iSQE/stm32f746gdisco-question

You will need to do the due-diligence on this. Review the circuits and signalling expectations.

If you can't make these determinations from available documentation, the answer is probably No, and you'll likely need to do the experiment and work up the code to come to a definitive answer. Or pay going rates for someone else to do the work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I'm using the STM32F429 Discovery board. I see from the schematic of this board that it is using a 18 bit RGB interface which is fine. Also, it looks like the LCD is connected via a 48 pin FFC connector.