cancel
Showing results for 
Search instead for 
Did you mean: 

MC workbench / STM32F303 LQFP48 : wrong pin map

tarzan2
Associate II

Hello,

Using the 48-pin variant (STM32F303CB), the "analog input and protection" pin mapper propose inputs that doesn't exist on the chip (C-port) and doesn't propose available pin (A1, A2, A3...)

Any workaround?

Thank you

3 REPLIES 3
Laurent Ca...
Lead II

Dear nicolasbouquet9

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear nicolasbouquet9

OK. I consider this post closed.

Do not hesitate to answer if it is not.

Best regards

Laurent Ca...

Hello Laurent,

Sorry to resurrect an old thread. I am actually having this same problem as well, with the STM32F303CB and the STM32G431 (I haven't tried with other chips). Any help would be greatly appreciated.

Also, do you know if the SDK will support more chips from the STM32G4 series anytime soon?

Erk