cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin5.44 lib missing GUI_SPLINE functions

APort
Associate III

Hello,

Latest version of STemWin as included in STM32Cube_FW_L4_V1.14.0 apparently missing GUI_SPLINE_* functions in the provided *.a libs but they are listed in header file (GUI.h) - which causes linking error.

We are working with STemWin_CM4_wc32_ot_ARGB.a in particular but others are missing it as well.

This is very important feature for us.

Is there newer version, or version with this feature working?

Thanks in advance

1 REPLY 1
CSage
Associate

Hej,

Could you solve this issue?

I´m using STM32Cube_FW_F4_V1.24.2. This results into the same issue. I´m also using the same lib STemWIN_CM4_OS_wc32_ot_ARGB.a.