cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B with antenna size 30x30cm

Hzhao.2186
Associate II

Hi,

I am trying to design NFC antenna with ST25R3911B,the antenna size is about 30*30cm,and the read range need 35cm;

I want to know the target matching impedance ,and is it possible to fulfill this requirement with the ST25R3911B NFC reader?

1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

​Hello Sky,

Following this two threads, you should succeed.

https://community.st.com/s/question/0D50X0000AvgiHoSQI/st25r3911b-with-antenna-size-30x40cm

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

In the second thread we achieved a read range of 24cm using a 14x10 cm antenna. For you purpose I would recommend a 25x25cm or 30x30 cm antenna.

The Register 0x27 should be kept at 0x00. I would start with a target matching impedance around 15 to 20. The Q-factor should be around 35. The capacitive voltage divider should be setup in a way you achieve 2.7Vpp on the RFI (using the Measure Amplitude command).

Further information can be found in the application note "AN4974 Antenna matching for ST25R3911B/ST25R391x devices".

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

​Hello Sky,

Following this two threads, you should succeed.

https://community.st.com/s/question/0D50X0000AvgiHoSQI/st25r3911b-with-antenna-size-30x40cm

https://community.st.com/s/question/0D50X00009XkWCSSA3/design-questions-around-st25r3911b

In the second thread we achieved a read range of 24cm using a 14x10 cm antenna. For you purpose I would recommend a 25x25cm or 30x30 cm antenna.

The Register 0x27 should be kept at 0x00. I would start with a target matching impedance around 15 to 20. The Q-factor should be around 35. The capacitive voltage divider should be setup in a way you achieve 2.7Vpp on the RFI (using the Measure Amplitude command).

Further information can be found in the application note "AN4974 Antenna matching for ST25R3911B/ST25R391x devices".

BR Travis