cancel
Showing results for 
Search instead for 
Did you mean: 

MBEDTLS HANDSHAKE_FAILURE on STM3210C board

Zanon.Luciano
Senior

Hi, I’m trying to establish TLS communication with my local mosquitto broker.

The handshake always fails, the broker does not accept the hello client and I cannot understand why …

Below the decoded messages that pass over the network.

Messages are captured with wireshark:

Secure Sockets Layer

  TLSv1.2 Record Layer: Handshake Protocol: Client Hello

    Content Type: Handshake (22)

    Version: TLS 1.2 (0x0303)

    Length: 81

    Handshake Protocol: Client Hello

      Handshake Type: Client Hello (1)

      Length: 77

      Version: TLS 1.2 (0x0303)

      Random

      Session ID Length: 0

      Cipher Suites Length: 6

      Cipher Suites (3 suites)

        Cipher Suite: TLS_ECDHE_ECDSA_WITH_AES_256_GCM_SHA384 (0xc02c)

        Cipher Suite: TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256 (0xc02b)

        Cipher Suite: TLS_EMPTY_RENEGOTIATION_INFO_SCSV (0x00ff)

      Compression Methods Length: 1

      Compression Methods (1 method)

        Compression Method: null (0)

      Extensions Length: 30

      Extension: signature_algorithms

        Type: signature_algorithms (0x000d)

        Length: 10

        Signature Hash Algorithms Length: 8

        Signature Hash Algorithms (4 algorithms)

          Signature Hash Algorithm: 0x0603

          Signature Hash Algorithm: 0x0503

          Signature Hash Algorithm: 0x0403

          Signature Hash Algorithm: 0x0303

      Extension: elliptic_curves

        Type: elliptic_curves (0x000a)

        Length: 6

        Elliptic Curves Length: 4

        Elliptic curves (2 curves)

          Elliptic curve: secp384r1 (0x0018)

          Elliptic curve: secp256r1 (0x0017)

      Extension: ec_point_formats

        Type: ec_point_formats (0x000b)

        Length: 2

        EC point formats Length: 1

        Elliptic curves point formats (1)

          EC point format: uncompressed (0)

config.h is the “suite-b�? proposed by Mbed …

I also tried to configure the mosquitto broker with “ciphers ALL�? but nothing changed …

The broker’s response is always the following:

Secure Sockets Layer

  TLSv1.2 Record Layer: Alert (Level: Fatal, Description: Handshake Failure)

    Content Type: Alert (21)

    Version: TLS 1.2 (0x0303)

    Length: 2

    Alert Message

      Level: Fatal (2)

      Description: Handshake Failure (40)

is there anyone who can help me?

0 REPLIES 0