cancel
Showing results for 
Search instead for 
Did you mean: 

HI I have Steval ESC001v1. And i wand to drive a bldc moter throught PWM control signal. i have install the latest X-Cube MCSDK v5.4.1 and STM32 Cube MX v5.4.0 and IAR EWARM 8. i am new on STM Controllers so Kindly Guid me acordingle.

Nain
Associate

The Motor runs correctly when i am driving it from serial through MC WB. but i want to drive the motor from PWM.

Any Help Plz...

2 REPLIES 2
TGull.1
Associate II

Hi Nain,

did you manage to resolve this issue please?

I have a similar toolchain setup (albeit a couple of slightly updated versions) and get the same response.

Motor runs perfectly under ST Motor Profiler and ST MC Workbench, but when code is generated for EWARM 8, compiled and pushed out onto the chip there is no response to 490Hz PWM input with 1240us duty.

Any indication of how you corrected the setup/ configuration/process would be greatly appreciated.

Regards

Tim

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards