2019-11-07 04:29 AM
2019-11-07 04:35 AM
2019-11-07 06:51 AM
Yes, but don't expect it to get through any router unless you create proper TCP/IP packets.
2019-11-07 07:58 AM
should get to all nodes connected to the switch(s)/hub(s) within the "ethernet" segment you have wired together.
Ask simple questions, get simple answers.
Yes, the LWIP stack sits on top of stuff that just sends/receives on the Ethernet, you can remove LWIP and "Just Do It!"(TM)
2019-11-07 11:15 PM
Can anyone provide the code for the same (sending and receiving packets using STM32H743) without using LWIP. Please recommend the software for testing the same.