cancel
Showing results for 
Search instead for 
Did you mean: 

Hi ! When the boot mode activated in STM32F427VIT6 ( BOOT0 pin to HIGH level) , the pin PE13 in strong HIGH state

OLe.812
Associate II

When the boot mode activated in STM32F427VIT6 ( BOOT0 pin to HIGH level) , the pin PE13 in strong HIGH state (really 3.3V). Why? The PE13 pin goes to LOW level just if i begin download firmware by UART bootloader

4 REPLIES 4

> ( BOOT0 pin to HIGH level) , the pin PE13 in strong HIGH state

What is connected to PE13?

Also, is it going to HIGH immediately after NRST ends? (observe with an oscilloscope).

JW

OLe.812
Associate II

To PE13 just coonected 10k resistor to GND and thats it. Yes, PE13 still in HIGH after reset, look the attached picture from scope . Thanks for you reply:)

NRST is active low, at that moment all pins are Hi-Z by the processor.

So why is PE13 actually higher during NRST low, if it's just a 10k resistor to GND?

The 2.4V after reset ends is suspicious, too, though.

JW

OLe.812
Associate II

Yes. its higher during NRST low... and it state of PE13 will be switch on MOSFET with current 1A in my circuit (if i connect this pin)