cancel
Showing results for 
Search instead for 
Did you mean: 

Migrate IOC file from older MX to CubeIDE

fsch
Associate III

I have an IOC file from an older CubeMX. Since I could not find the MX version number in either mxproject or ioc file, I cannot tell the exact version. It should be about one or two years old.

Now I want to open it in MX 5.4 from CubeIDE 1.1.

MX asks to migrate the file, which I do but then the project has a lot of errors in its configuration and cannot generate code. Almost all items in the Connectivity section are conflicting with something. The IOC project is in production use with Atollic TRUESTudio so I doubt that it is broken.

Has anyone migrated an IOC file successfully and can give some advice?

Thank you.

0 REPLIES 0