cancel
Showing results for 
Search instead for 
Did you mean: 

Error/omission in RM0090: missing CC4NP bit definition

TDK
Guru

The CC4NP bit in the TIMx_CCER register should be listed in the reference manual in the section "17.4.9 TIM1 and TIM8 capture/compare enable register (TIMx_CCER)". Currently, only the CC1NP, CC2NP, and CC3NP bits are listed. The sections for the other timers correctly list this bit.

This bit is used when channel 4 is configured in input capture (IC) mode to help determine if triggers occur on rising and/or falling edges.

I checked the latest RM0090 (rev18) reference manual and the bit is not listed in there in this section.

https://www.st.com/resource/en/reference_manual/dm00031020.pdf

If you feel a post has answered your question, please click "Accept as Solution".
1 REPLY 1
Imen.D
ST Employee

Hello @TDK​ ,

You are right, we will correct this error for all impacted STM32F4 and STM32F2 reference manuals .

Thanks for bringing this to our attention.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen