cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: CubeMX fails to support timer PWM modes

Note: This is still broken in RubeMX 5.4.0

Note: I am using the CubeMX plug-in within the STM32CubeIDE, not the stand-alone CubeMX.

RubeMX shows only 5 of 7 possible timer channel modes. It fails to show PWM modes. Attached IOC shows problem (try to set PWM mode for timer 1 or timer 3).

STM32CubeIDE Version: 1.1.0

Build: 4551_20191014-1140 (UTC)

OS: Windows 10, v.10.0, x86_64 / win32

Java version: 1.8.0_202

Please confirm you have reproduced this and filed a ticket...

Thanks, Best Regards, Dave

4 REPLIES 4
Khouloud ZEMMELI
ST Employee

​Hello @Dave Nadler​ , Issue has been fixed ,please switch to 5.4.0 CubeMX version.

0690X00000AqikWQAR.png

best Regards,

Khouloud.

Khouloud Zemmeli (ST Employee) - As I wrote above, I am trying to use STM32CubeIDE Version: 1.1.0. Are you saying this bug is fixed in the stand-alone CubeMX, but not the CubeMX included in ST's IDE??

​Strating your project from CubeMX (5.4.0) or CubeIDE (1.1.0) , Same result , the PWM mode is supported .

Best Regrads,

Khouloud.

@Khouloud ZEMMELI​ - This bug is still not fixed. I just tried again in CubeIDE after updating all MX definitions.

The PWM options are still missing.

The generated report says

STM32CubeMX 	5.4.0
Date	10/25/2019
MCU	STM32F413CGUx