cancel
Showing results for 
Search instead for 
Did you mean: 

Error when creating applications

Henrik C
Associate II

When I try to create a project for a Discovery Kit or open the online application in TouchGFX Designer, the "Downloading Application Template" and "Downloading GUI" slowly reach 100% and then this error screen is displayed:

/*

Sorry - something unexpected has happened which caused an error to occur in the Designer.

For more information, see the log file located at: C:\Users\User\AppData\Roaming\TouchGFX-4.12.3\TouchGFXDesigner.log

Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.

You can find the Help Center here: http://support.touchgfx.com

Error: Värde får inte vara null.

Parameternamn: stream

*/

It appears to give the same error whichever board I choose and any Demo template. Same for both My Applications and Online Applications.

Looking in the referenced log file I find this:

[1] ERROR TouchGFXDesigner.App: Värde får inte vara null.

Parameternamn: stream

System.ArgumentNullException: Värde får inte vara null.

Parameternamn: stream

  vid System.IO.Compression.ZipArchive..ctor(Stream stream, ZipArchiveMode mode, Boolean leaveOpen, Encoding entryNameEncoding)

  vid TouchGFXPackages.PackageManager.Unpack(TouchGFXPackage touchGFXPackage, String projectPath, String applicationName, Action`2 progress)

  vid TouchGFXPackages.PackageManager.CombineAtAndUi(TouchGFXPackage tgui, TouchGFXPackage tgat, String projectPath, String applicationName, Int32 height, Int32 width, ColorDepth selectedColorDepth, Action`2 progress)

  vid TouchGFXDesigner.Main.StartupWindow.MyApplications.CreateNewApplicationViewModel.b__0()

  vid System.Threading.Tasks.Task`1.InnerInvoke()

  vid System.Threading.Tasks.Task.Execute()

--- **** på stackspårningen från föregående plats där ett undantag utlöstes ---

  vid System.Runtime.CompilerServices.TaskAwaiter.ThrowForNonSuccess(Task task)

  vid System.Runtime.CompilerServices.TaskAwaiter.HandleNonSuccessAndDebuggerNotification(Task task)

  vid TouchGFXDesigner.Main.StartupWindow.MyApplications.CreateNewApplicationViewModel.d__81.MoveNext()

--- **** på stackspårningen från föregående plats där ett undantag utlöstes ---

  vid System.Runtime.CompilerServices.TaskAwaiter.ThrowForNonSuccess(Task task)

  vid System.Runtime.CompilerServices.TaskAwaiter.HandleNonSuccessAndDebuggerNotification(Task task)

  vid TouchGFXDesigner.Main.StartupWindow.MyApplications.CreateNewApplicationViewModel.d__44.MoveNext()

--- **** på stackspårningen från föregående plats där ett undantag utlöstes ---

  vid System.Runtime.CompilerServices.AsyncMethodBuilderCore.b__6_0(Object state)

  vid System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)

  vid System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)

1 REPLY 1
Martin KJELDSEN
Chief III

Hi,

Something could've happened in the download of the file. Try deleting your %APPDATA%/TouchGFX-4.12.3\Downloads folder - This will force a re-download. You could also just delete the package in question from that folder.

/Martin