cancel
Showing results for 
Search instead for 
Did you mean: 

Error in RM0440 Rev 1 and 2

TKrop
Associate II

On page 92, table 7 contains flash memory addresses and their sizes.

For every address range, the difference between the start and end address is 0x7FF, i.e. 2 KiB.

However, for Page 127 in both Bank 1 and Bank 2, the range is listed to be 0xFFF, i.e. 4 KiB.

The error here is that both starting addresses should end with '800' instead of '000'.

Additionally, table 8 is missing a hyphen on its Page 127 address range.

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello,

You are right, this should be corrected: Page 127 range in Table7 is:

0x0803 F800 - 0x0803 FFFF.

0x0807 F800 - 0x0807 FFFF.

We will correct this in the next RM0440 release.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello,

You are right, this should be corrected: Page 127 range in Table7 is:

0x0803 F800 - 0x0803 FFFF.

0x0807 F800 - 0x0807 FFFF.

We will correct this in the next RM0440 release.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen