cancel
Showing results for 
Search instead for 
Did you mean: 

VL6180X measured distance is dependent on specularity of the target surface

BLudi
Associate

I am evaluating the VL6180X to be used in a microtiter plate detector device and have noticed the measured distance is significantly underestimated for specular/mirroring/glossy surfaces. Furthermore the results is stronglly dependent on the angle. If the surface is tilted along the long axis of the VL6180X, the measured distance increases both when its tilted to the right or to left. If the surface id tilted along the short axis of the VL6180X, the measured distance very stronly increases or decreases depending on the tilting direction. The effect is much larger than what could possibly be explained by simple geometry (and tilting matted surface has basically no effect).

What is the reason for these effects ? Can they be attenuated/eliminated or compensated for?

1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

The Vertical Cavity Surface Emitting Laser (VCSEL) used has a limitation. The main bit of light that illuminates the center region of the cone starts just a touch ahead of the outer region. Generally this is not an issue, as the mathematical model used takes this into account. But for very reflective surfaces smooth the model breaks down a bit and there is a small offset. It is this effect you are seeing.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.

View solution in original post

2 REPLIES 2
John E KVAM
ST Employee

The Vertical Cavity Surface Emitting Laser (VCSEL) used has a limitation. The main bit of light that illuminates the center region of the cone starts just a touch ahead of the outer region. Generally this is not an issue, as the mathematical model used takes this into account. But for very reflective surfaces smooth the model breaks down a bit and there is a small offset. It is this effect you are seeing.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.
BLudi
Associate

Is this problem solved in the new VL53L3CX?