2019-10-04 02:50 AM
Hi,
I am using STM32l4 nucleo-144 board to create an example application for LPUART1 communication.
Part number - STM32L4R5ZI
I have configured the GPIO and required clocks. But still not able to do a successful transaction.
/* Enable Power Clock */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
/* Ensure that HSI is wake-up system clock */
LL_RCC_SetClkAfterWakeFromStop(LL_RCC_STOP_WAKEUPCLOCK_HSI);
/*##### -1- Enable peripherals and GPIO Clocks #####*/
/* Enable GPIO TX/RX clock */
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOG);
/* Configure TX Pin as : Alternate function, High Speed, PushPull, Pull up */
LL_GPIO_SetPinMode(GPIOG, LL_GPIO_PIN_7, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_8_15(GPIOG, LL_GPIO_PIN_7, LL_GPIO_AF_8);
LL_GPIO_SetPinSpeed(GPIOG, LL_GPIO_PIN_7, LL_GPIO_SPEED_FREQ_VERY_HIGH);
LL_GPIO_SetPinOutputType(GPIOG, LL_GPIO_PIN_7, LL_GPIO_OUTPUT_PUSHPULL);
LL_GPIO_SetPinPull(GPIOG, LL_GPIO_PIN_7, LL_GPIO_PULL_NO);
/* Configure RX Pin as : Alternate function, High Speed, PushPull, Pull up */
LL_GPIO_SetPinMode(GPIOG, LL_GPIO_PIN_8, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_8_15(GPIOG, LL_GPIO_PIN_8, LL_GPIO_AF_8);
LL_GPIO_SetPinSpeed(GPIOG, LL_GPIO_PIN_8, LL_GPIO_SPEED_FREQ_VERY_HIGH);
LL_GPIO_SetPinOutputType(GPIOG, LL_GPIO_PIN_8, LL_GPIO_OUTPUT_PUSHPULL);
LL_GPIO_SetPinPull(GPIOG, LL_GPIO_PIN_8, LL_GPIO_PULL_NO);
/* Enable SPI clock */
/* Initialize LPUART instance according to parameters defined in initialization structure */
LL_LPUART_Init(LPUART1, &nucleoLpuartStruct);
/* Set the wake-up event type : specify wake-up on RXNE flag */
LL_LPUART_SetWKUPType(LPUART1, LL_LPUART_WAKEUP_ON_RXNE);
/*##### -2- Configure peripheral GPIO #####*/
LL_APB1_GRP2_EnableClock(LL_APB1_GRP2_PERIPH_LPUART1);
/* Set LPUART1 clock source as HSI */
LL_RCC_SetLPUARTClockSource(LL_RCC_LPUART1_CLKSOURCE_HSI);
/*##### -3- NVIC Configuration for LPUART1 interrupts #####*/
/* - Set priority for LPUART1_IRQn */
/* - Enable LPUART1_IRQn */
NVIC_SetPriority(LPUART1_IRQn, 0);
NVIC_EnableIRQ(LPUART1_IRQn);
LL_LPUART_Enable(LPUART1);
Is there any example code available for LPUART of STM32L4R5ZI board ?
Thanks & Regards,
Shanmathi P
Solved! Go to Solution.
2019-10-04 03:55 AM
2019-10-04 03:55 AM
2019-10-04 04:55 AM
Hi Clive,
I have added LL_PWR_EnableVddIO2(); API call.
Still communication is not success.
It would be great if you could share the example code for this board.
2019-10-04 05:25 AM
2019-10-04 08:09 AM
I'm not using LL, but this is what works for me.
/* IOSV bit MUST be set to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddIO2();
//****************************************************************************
void LPUART1_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = { 0 };
__LPUART1_CLK_ENABLE();
__GPIOG_CLK_ENABLE();
/* UART RX/TX GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_7 | GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF8_LPUART1;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
/*## Configure the UART peripheral ######################################*/
/* Put the USART peripheral in the Asynchronous mode (UART Mode) */
/* UART1 configured as follow:
- Word Length = 8 Bits
- Stop Bit = One Stop bit
- Parity = NO parity
- BaudRate = 115200 baud
- Hardware flow control disabled (RTS and CTS signals) */
UartHandle.Instance = LPUART1;
UartHandle.Init.BaudRate = 115200;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
#ifdef UART_ONE_BIT_SAMPLE_DISABLE
UartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
#endif
if (HAL_UART_Init(&UartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
// HAL_NVIC_SetPriority(LPUART1_IRQn, 1, 0);
// HAL_NVIC_EnableIRQ(LPUART1_IRQn);
}
//****************************************************************************
The availability of LL specific examples for the board is low, you could fund some work if you need some.
If think you enable the LPUART1 clock too late in your original post
2019-10-10 04:50 AM
Thanks @Community member .
I am now able to send data via LPUART successfully, after implementing the above suggestions.
2019-10-15 04:39 AM
Hi @Community member ,
The data transmission and reception is fine when connected via the virtual com port.
But when I try to connect the GPIO pins via a USB to UART converter, only TX from the nucleo board works. RX data from PC to board is not received. Is there any additional configuration or hardware changes required?