cancel
Showing results for 
Search instead for 
Did you mean: 

Incorrect color of standard buttons. png with transparent background. What is wrong?

lexabps
Associate II

Hi.

The problem is

The project is in the memory of mcu (flash).

button - OK

0690X000009jsG9QAI.jpg

0690X000009jsGJQAY.jpg

The project is in the memory of QUADSPI.

0690X000009jsHCQAY.jpg

0690X000009jsHRQAY.jpg

what could be the problem?

Добрый день.

Проблема �?ледующа�?...

Е�?ли пиши проект в mcu, отображает�?�? корректно. Е�?ли на флешку, то пропадает цвет кнопок.

Что может быть не так �? проектом???

Видео и проект во вложение.

4 REPLIES 4
lexabps
Associate II

All PNG files from the toucgfx demo project0690X000009jxbWQAQ.jpg

Hello,

I see you are using a custom hardware (QSPI W25Q128 and others). Did you run sort of validation tests to make sure writing and reading from the QSPI is fine?

With regards,

Badreddine

0690X000009jytvQAA.jpg

test project

These files are displayed correctly.

0690X000009jyutQAA.png

0690X000009jyv3QAA.png

These files are not displayed correctly.

(png with transparent background)

0690X000009jywGQAQ.png0690X000009jyw6QAA.png0690X000009jyw1QAA.png