cancel
Showing results for 
Search instead for 
Did you mean: 

I had short circuit between +5V and GND. And i get 'usb did not recognized' error. What should i do?

ahmetgunduz
Associate III

Hi,

i'm using STM32F40G DISVOVERY board. when i measue D1 i see 2.5 volt. Also when i measure 5V pin, i see 2.5 volt. What should i do? Can replacing D1 by D2 solve the problem?

2 REPLIES 2
TDK
Guru

You should fix the short and ensure the power scheme is working correctly first. Likely the chip is fine but something upstream may have failed.

The discovery boards shouldn’t have power issues. Is yours modified or do you know why it may have failed?

If you feel a post has answered your question, please click "Accept as Solution".

Yes, its my fault. I connected 5v to GND unknowingly.

How can i ​ensure the power scheme is working. I am a newbie. Can you send me a link, please?