cancel
Showing results for 
Search instead for 
Did you mean: 

How to program data to the QSPI NOR memory (MT25QL256, 32MB)?

JNguyen
Senior

My board has QSPI NOR memory (MT25QL256, 32MB) and STM32H750. I used Studio, CubeMX and CubeProgrammer to work with QSPI external memory on F746G-Disco board with no problem. But I have problem on my board with QSPI. My H750-MT25QL schm is same as in Disco board. Software is generated by CubeMX. Attached are .ioc, linker, map, start-up script error msg.

I have this attribute for the table I want to place in QSPI:

__attribute__((section(".imgqspi")))

const uint16_t image_data_Kidman120x160[19200] = {0x00, ...}

I probed MT25Q's CLK and CS pins while CubeProg was programming the board. There were no activities. It seems like H750 was not talking to MT25. I think I miss some start-up setting for the MCU.

7 REPLIES 7

QSPI is at 0x90000000 not 0x09000000

You'd need to specify a workable External Loader to manage ICs / Interface beyond the pins on the STM32

09:31:54 : Size : 1024 Bytes

09:31:54 : Address : 0x9000000 <- on the STM32 Cube Programmer side

09:31:54 : Read progress:

09:31:54 : Error: Data read failed

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
JNguyen
Senior

That's what I'm looking for "a workable External Loader to manage ICs / Interface." How do I create it? I've read some AN from ST about dev_inf.h and Loader_src.c, but can't follow it completely.

Below is the log from CubeProg, which has the correct address 0x90000000. The problem occurs when CubeProg gets to the external memory.

08:24:44 : ST-LINK SN : 52FF6E067266535551540867

08:24:44 : ST-LINK FW : V2J31S7

08:24:44 : Voltage : 1.80V

08:24:44 : SWD freq : 4000 KHz

08:24:44 : Connect mode: Normal

08:24:44 : Reset mode : Software reset

08:24:44 : Device ID : 0x450

08:24:45 : UPLOADING OPTION BYTES DATA ...

08:24:45 : Bank : 0x00

08:24:45 : Address : 0x5200201c

08:24:45 : Size : 308 Bytes

08:24:45 : UPLOADING ...

08:24:45 : Size : 1024 Bytes

08:24:45 : Address : 0x8000000

08:24:45 : Read progress:

08:24:45 : Data read successfully

08:24:45 : Time elapsed during the read operation is: 00:00:00.007

08:24:53 : Read File: C:\Users\...\Documents\Projects\...\...\Debug\Vue0.1.hex

08:24:53 : Number of segments: 2

08:24:53 : segment[0]: address= 0x8000000, size= 0x10848

08:24:53 : segment[1]: address= 0x90000000, size= 0x9600

08:25:07 : Memory Programming ...

08:25:07 : Opening and parsing file: Vue0.1.hex

08:25:07 : File : Vue0.1.hex

08:25:07 : Size : 106056 Bytes

08:25:07 : Address : 0x08000000 

08:25:07 : Erasing memory corresponding to segment 0:

08:25:12 : Erasing memory corresponding to segment 1:

08:25:12 : Erasing external memory sector 0

08:25:17 : Error: failed to erase memory

08:25:17 : Error: failed to erase memory

Enumerate the specific pins and AF selection for the QSPI interface. Or attach the BSP implementation that works with your board.

First step would be to have workable QSPI access code in your own application. Build a framework capable of Erase, Write and Read functionality.

Review Keil's documentation for Flash Algorithms, the ST External Loader design is modelled on that design. Implement you own loader, perhaps build a wrapper around the Loader functionality so you can test/evaluate outside of the Cube Programmer. If you have an available USART you can use this to understand/debug the loader once it is running under Cube Programmer.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
JNguyen
Senior

My code is simple and tested OK on 32F746G-Disco board: storing LCD image on QSPI, and MCU to copy to LCD. So QSPI access code is there. My QSPI accessing code is based from codes of 32F746G-Disco. If I don't store data in QSPI, my code initializes MT25QL256ABAEW9 without error.

32F746G-Disco has memory part N25Q128A which is pin compatible to the memory part MT25QL256ABAEW9 on my board, only diff capacities. CubeProg has N25Q128A part in the list of external memory devices, but not MT25QL256ABAEW9. So first step is how do I fix this? Attached are files STM32H750VB_FLASH.ld and Dev_Inf.h. What do I miss?

Cube Programmer only lists the devices it can find in its ExternalLoader subdirectory

I don't think the issue relates to the linker script, and the Dev_Inf simply describes the capacity and geometry of the device, the real magic is in the body of the loader itself and its initialization and use of the memory device.

This really isn't something I can explain/tutorialize in 5 mins or less. Also looks like I'm going to have to determine the exact pins myself.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
JNguyen
Senior

I had this solved. See my other post "How to create CubeProg stldr loader file for QSPI external memory?"

The other thread to which you are referring.

https://community.st.com/s/question/0D50X0000BaMXDTSQ4/how-to-create-cubeprog-stldr-loader-file-for-qspi-external-memory

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..