cancel
Showing results for 
Search instead for 
Did you mean: 

Definitions or exact meaning for signal rate and other parameters

SatyaK
Associate

Hi,

We are using VL53L5 TOF sensor for our development,

Unit for signal rate is MCPS (mega counts per seconds). What exactly is it counting?

Is it measure of intensity of signal received? Does it mean that, Higher the signal rate, higher is intensity of received signal. Does higher signal rate means good confidence is reported range.

Thanks,

Satya

2 REPLIES 2
John E KVAM
ST Employee

​All the VL53 sensors measure signal strength in MegaCounts per second - And each PHOTON received is a count. 20million is about as high as we go. After that we start turning off SPADs (the photon detectors) to lower the strength. Anything above 0.5 MCPS will produce an answer depending on ambient and a few other conditions.

  • john

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.
John E KVAM
ST Employee

​One further note. On the VL53L0 and L1 signal strength is the total number of counts received. One really needs to divide that by the number of SPAD photon detectors used and then normalized by multiplying by 200. Then one can compare the signal strength from one measurement to another. (On the VL6180 we always use the same number of SPADs.)


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.