cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769 (STM32F769I-DISCO) \USB_Device\MSC_Standalone\ Example doesn't run

TTimm
Associate II

Hi,

I try to get the Device-MSC_Standalone run.

It should be play, out of the box.

When I plug the USB-Connector (CN15) to the PC,

an error occur.

Windows-Dev-Maanager stated:

"Error while request Device-Descrpitor"

What is wrong?

Compiler-Option "USE_USB_HS" is never used in the Code.

The Example is based on "STM32Cube_FW_F7_V1.15.0".

see readme.txt

This application has been tested with STMicroelectronics STM32F769I-Discovery...

In the Example-Dir of STM32Cube_FW_L4_V1.14.0.../32L496GDISCOVERY

there is no "MSC-Standalone" at all.

Why not?

Kind Regards

Thomas

1 REPLY 1
TTimm
Associate II

OK, no answers but new informations...

when connected to PC with OS Windows 7 a STM-Drive appears

and is read-/writeable. (disk.sys/partmgr.sys will be used)

when connected to PC with OS Windows 10,

no driver will be found :(

Is this a common Windows Problem?

Any Recommendation which Driver should be used?

Kind regards

Thomas