2019-09-20 03:00 PM
I have tried with and without the Cube generated code but no luck getting LPUART to send any printable characters/bytes to an external TeraTerm terminal over VCOM.
I think I am missing some clocking or initialization step -- any help is appreciated.
Cheers
Ramanand
// ########################
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_LPUART1_UART_Init();
}
return;
}
2019-09-20 03:01 PM
The webpage would not let me add all my code -- is there a mechanism to attach code snippets to this thread?
2019-09-20 05:09 PM
2019-09-20 05:22 PM
NUCLEO-L496ZG sourcer32@gmail.com
/* ## Definition of UARTx related resources ################################### */
/* Definition of UARTx */
#define UARTx LPUART1
/* Definition of UARTx clock resources */
#define UARTx_CLK_ENABLE() __HAL_RCC_LPUART1_CLK_ENABLE()
#define UARTx_TX_PIN_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
#define UARTx_RX_PIN_CLK_ENABLE() __HAL_RCC_GPIOG_CLK_ENABLE()
/* Definition of UARTx channels pins */
#define UARTx_TX_PIN GPIO_PIN_7
#define UARTx_TX_GPIO_PORT GPIOG
#define UARTx_TX_AF GPIO_AF8_LPUART1
#define UARTx_RX_PIN GPIO_PIN_8
#define UARTx_RX_GPIO_PORT GPIOG
#define UARTx_RX_AF GPIO_AF8_LPUART1
/**
* @brief UART MSP Init
* @param huart: uart handle
* @retval None
*/
void HAL_UART_MspInit(UART_HandleTypeDef *huart)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Enable UARTx GPIO TX/RX clock */
UARTx_TX_PIN_CLK_ENABLE();
UARTx_RX_PIN_CLK_ENABLE();
/* Enable UARTx clock */
UARTx_CLK_ENABLE();
/* IOSV bit MUST be set to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddIO2();
/* Configure UARTx Rx and Tx as alternate function */
GPIO_InitStruct.Pin = UARTx_TX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = UARTx_TX_AF;
HAL_GPIO_Init(UARTx_TX_GPIO_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = UARTx_RX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = UARTx_RX_AF;
HAL_GPIO_Init(UARTx_RX_GPIO_PORT, &GPIO_InitStruct);
}
/* UART handler declaration */
UART_HandleTypeDef UartHandle;
#ifdef __GNUC__
/* With GCC, small printf (option LD Linker->Libraries->Small printf
set to 'Yes') calls __io_putchar() */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#else
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#endif /* __GNUC__ */
/**
* @brief UART Configuration
* @param None
* @retval None
*/
/*
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Tx and Rx enabled
*/
static void UART_Config(void)
{
UartHandle.Instance = UARTx;
UartHandle.Init.BaudRate = 115200;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
UartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
if(HAL_UART_Init(&UartHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
}
/**
* @brief Retargets the C library printf function to the UART.
* @param None
* @retval None
*/
PUTCHAR_PROTOTYPE
{
/* Place your implementation of fputc here */
/* e.g. write a character to the EVAL_COM1 and Loop until the end of transmission */
HAL_UART_Transmit(&UartHandle, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}