cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429, external interrupt errata?

MSipo
Senior II

External interrupt errata?

I have setup EXTI_Line12 and EXTI_Line14 to generate en interrupt.

But the EXTI15_10_IRQHandler() fails to execute a second interrupt if it happens too close to the first interrupt.

But it seems only happen when I use bit-banding to check and clear the bits in the EXTI->PR register. If I access the EXTI->PR directly at the normal address it does not happen.

Is this a known problem?

I read something similar in another chip errata (but on an STM8):

When an interrupt handler starts executing a service routine and an external interrupt (EXTI) request is pending or arrives during the same cycle, the external interrupt is not executed.

void EXTI15_10_IRQHandler(void)
{
    GPIO_SetBits(GPIOB, GPIO_Pin_10); // Toggle PB10 to show we are entering the interrupt
    GPIO_ResetBits(GPIOB, GPIO_Pin_10);
 
    // NOTE:
    //  PERIPH_GET_BIT is a macro that reads one bit using bit-banding
    //  PERIPH_SET_BIT is a macro that sets a bit using bit-banding
 
#ifdef USE_BIT_BANDING
    if (PERIPH_GET_BIT(EXTI->PR, EXTI_Line12))
#else
    if (EXTI->PR & EXTI_Line12)
#endif
    {
        // Clear the EXTI line pending bit
#ifdef USE_BIT_BANDING
        PERIPH_SET_BIT(EXTI->PR, EXTI_Line12);
#else
        EXTI->PR = EXTI_Line12;
#endif
        // Keep PB10 high as long as we do stuff A
        GPIO_SetBits(GPIOB, GPIO_Pin_10);
        do_stuff_a();
        GPIO_ResetBits(GPIOB, GPIO_Pin_10);
    }
 
#ifdef USE_BIT_BANDING
    if (PERIPH_GET_BIT(EXTI->PR, EXTI_Line14))
#else
    if (EXTI->PR & EXTI_Line14)
#endif
    {
        // Clear the EXTI line pending bit
#ifdef USE_BIT_BANDING
        PERIPH_SET_BIT(EXTI->PR, EXTI_Line14);
#else
        EXTI->PR = EXTI_Line14;
#endif
        // Keep PB10 high as long as we do stuff B
        GPIO_SetBits(GPIOB, GPIO_Pin_10); 
        do_stuff_b();
        GPIO_ResetBits(GPIOB, GPIO_Pin_10);
    }
}

1 ACCEPTED SOLUTION

Accepted Solutions

You are not supposed to use a read-modify-write to clear the EXTI->PR bit, you should use a direct write. Bit-bandig writes are internally read-modify-write.

While this writeup is focused on the timer, the point is the same. (Sorry for the formatting, messed up courtesy of ST's forum software migration.)

JW

View solution in original post

3 REPLIES 3
Ozone
Lead

If I remember correctly, there was a race condition problem when you cleared an interrupt flag late in the handler, while another instance happened.

This is AFAIK a core-related issue (ARM), not STM32 related.

​Yes, I know. I hade that problem in a timer interrupt where I only cleared the interrupt flag and toggle an IO-pin. I needed to insert a dummy read/write access to a variable before leaving the interrupt to let the interrupt flag get time to clear.

You are not supposed to use a read-modify-write to clear the EXTI->PR bit, you should use a direct write. Bit-bandig writes are internally read-modify-write.

While this writeup is focused on the timer, the point is the same. (Sorry for the formatting, messed up courtesy of ST's forum software migration.)

JW