cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to execute MI command. GDB server doesn't initiate on macos mojave 10.14.6

ASilv.10
Associate

Hello,

I recently updated my OS (from OSX High Sierra to OS Mojave) and the gdb server stopped working.

Unfortunately there isn't many logs regarding what happened, all I get is an error message in a pop-up window saying that it failed to find the directory "localhost" which is pretty weird and doesn't make much sense to me.

I also attached an image of the pop-up window and my OS version in case it might help. Bellow there is the output of the IDE's console.

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Waiting for debugger connection...

Has anyone encountered this problem before?

0 REPLIES 0