2019-08-28 01:37 PM
Hello,
is there any example how to configure LTDC device tree entry for RGB display ?
Documentation is unclear on that, only MIPI mode is quite well documented.
Regards
Arkadiusz
Solved! Go to Solution.
2019-08-29 06:00 AM
On the boards DK1 and DK2 the LTDC output is connected to the HDMI transmitter sil sii9022
This is a first example of using LTDC, but not exactly what you want.
On board EV1 there is an empty connector for LTDC. I have used it to test some RGB LCD panels described in Linux driver panel-simple.c
These are the lines I have added at the end of stm32mp157c-ev1.dts
With the information in the datasheet of the panel is not difficult to add a new entry in panel-simple.c
/* disable DSI panel */
&dsi {
status = "disabled";
};
/* connect LTDC to the panel */
<dc {
port {
ltdc_ep1_out: endpoint@1 {
reg = <1>;
remote-endpoint = <&panel_rgb_in>;
};
};
};
/* simple-panel on LTDC */
/ {
panel-rgb@0 {
compatible = "ampire,am-480272h3tmqw-t01h", "simple-panel";
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_b>;
pinctrl-1 = <<dc_pins_sleep_b>;
port {
panel_rgb_in: endpoint {
remote-endpoint = <<dc_ep1_out>;
};
};
};
};
2019-08-29 12:14 AM
Hi,
Did you look at https://wiki.st.com/stm32mpu/wiki/LTDC_device_tree_configuration ?
DPI/RGB bindings are in https://github.com/STMicroelectronics/linux/blob/v4.19-stm32mp/Documentation/devicetree/bindings/display/st,stm32-ltdc.txt
Regards
2019-08-29 06:00 AM
On the boards DK1 and DK2 the LTDC output is connected to the HDMI transmitter sil sii9022
This is a first example of using LTDC, but not exactly what you want.
On board EV1 there is an empty connector for LTDC. I have used it to test some RGB LCD panels described in Linux driver panel-simple.c
These are the lines I have added at the end of stm32mp157c-ev1.dts
With the information in the datasheet of the panel is not difficult to add a new entry in panel-simple.c
/* disable DSI panel */
&dsi {
status = "disabled";
};
/* connect LTDC to the panel */
<dc {
port {
ltdc_ep1_out: endpoint@1 {
reg = <1>;
remote-endpoint = <&panel_rgb_in>;
};
};
};
/* simple-panel on LTDC */
/ {
panel-rgb@0 {
compatible = "ampire,am-480272h3tmqw-t01h", "simple-panel";
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_b>;
pinctrl-1 = <<dc_pins_sleep_b>;
port {
panel_rgb_in: endpoint {
remote-endpoint = <<dc_ep1_out>;
};
};
};
};
2019-08-30 11:52 AM
That helped, thx.
2021-05-26 02:27 AM
@AntonioST As this does not seem to work anymore after 2 years, could you please update your answer according to the latest device tree changes?
2021-06-06 10:10 AM
I was able to get my display working on openstlinux-5.10-dunfell-mp1-21-03-31 with the following code.
/* root */
panel {
compatible = "innolux,at070tn92";
enable-gpios = <&gpioe 12 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpioe 11 GPIO_ACTIVE_HIGH>;
//backlight = <&panel_backlight>;
status = "okay";
port@0 {
reg = <0>;
panel_in: endpoint {
remote-endpoint = <<dc_ep0_out>;
};
};
};
<dc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_mx>;
pinctrl-1 = <<dc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ltdc */
port {
#address-cells = <1>;
#size-cells = <0>;
ltdc_ep0_out: endpoint@0 {
reg = <0>;
remote-endpoint = <&panel_in>;
};
};
/* USER CODE END ltdc */
};
2022-03-21 04:13 AM
Hello everybody,
Thank you for this information, I can't use the "modetest" command, it doesn't seem to recognize the screen.
Are there any specific things to configure when using buildroot and an RGB screen in dpi?
# modetest
trying to open device 'i915'...failed
trying to open device 'amdgpu'...failed
trying to open device 'radeon'...failed
trying to open device 'nouveau'...failed
trying to open device 'vmwgfx'...failed
trying to open device 'omapdrm'...failed
trying to open device 'exynos'...failed
trying to open device 'tilcdc'...failed
trying to open device 'msm'...failed
trying to open device 'sti'...failed
trying to open device 'tegra'...failed
trying to open device 'imx-drm'...failed
trying to open device 'rockchip'...failed
trying to open device 'atmel-hlcdc'...failed
trying to open device 'fsl-dcu-drm'...failed
trying to open device 'vc4'...failed
trying to open device 'virtio_gpu'...failed
trying to open device 'mediatek'...failed
trying to open device 'meson'...failed
trying to open device 'pl111'...failed
trying to open device 'stm'...failed
trying to open device 'sun4i-drm'...failed
trying to open device 'armada-drm'...failed
trying to open device 'komeda'...failed
trying to open device 'imx-dcss'...failed
trying to open device 'mxsfb-drm'...failed
no device found
Thank you very much