2019-08-28 11:47 AM
Hi
I am using stm32CubeMx to set one gpio and then trying to execute the code. I have tried both Atollic and STM32IDE both give me an error somewhere is system memory.
Error: 1fffdab8: Failed to execute MI command:
-data-disassemble -s 536861368 -e 536861400 -- 2
Error message from debugger back end:
Cannot access memory at address 0x1fffdab8
I am using the STM32F030CCT6 MCU.
Code builds fine but does not even allow me to set a break in main.
Where I first experienced the problem was with code I merged with code of the STM32F030k6 MCU. The code would step to GPIO_init and then fail at a certain point. To try and debug I did a setup in the cube with only one IO selected as output and the rest I ticked as analog.
Solved! Go to Solution.
2019-08-28 12:44 PM
2019-08-28 12:44 PM
2019-08-29 04:37 AM
Thanks Clive Two.Zero
That seemed to work. I missed it.