cancel
Showing results for 
Search instead for 
Did you mean: 

Does input frequency matter for smooth digital calibration

Ismet
Associate

Hi, does input frequency have effect on the smooth digital calibration period since in the documentation(screenshot attached) it says the calibration is performed during a cycle of 2 to the power of 20 which amounts to frequency of 32.768 x 32 . Does this change when the input frequency is 40.000 since both frequencies are configured with prescalers to 1 Hz. If it does, would I need to perform different calculations for number of clock pulses I want to mask/add?

Thank you for your response.

0 REPLIES 0