cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 Nucleo - Example for observing advertising messages

Michael Bauer
Associate II

Hello,

I am new to BLE and the STM32WB55. I want to get to a point where I can use the Nucleo board (MB1355C) to receive advertising messages which contain data. I was looking at the BLE example repository. I also attended the ST workshop for this microcontroller. If I understand right, these examples are meant to run on the STM32WB55 acting as the Server/Broadcaster/Peripheral while a smartphone operates as the Client/Observer/Central. Does anyone know if there are any examples of the STM32WB55 operating as the Client/Observer/Central?

Thanks and I appreciate the help.

Michael

4 REPLIES 4
Vyacheslav
Senior II

Hi !

“P2Client�? in examples/BLE folder is full client/observer/central example.

Michael Bauer
Associate II

Hi Vyacheslav. Thank you for replying. I want to make sure I am looking in the right location. I am examining STM32Cube\Repository\STM32Cube_FW_WB_V1.1.1\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pClient. Is that the location that you meant? In there I only see the one example. Perhaps I am misunderstanding.

Hi, Michael.

Yes, you are right, if you need to learn a client - that is current path:

SDK_FOLDER\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pClient.

What you mean " one example" ?

Client, Observer, Central - it's almost the same thing but at different levels.

Central - on GAP level

Client - on GATT level

Observer - advertising level

If you want something specific, then tell me what exactly.

Regards,

Vyacheslav.

Remi QUINTIN
ST Employee

You may download the last STM32Cube_FW_WB_V1.2.0​ FW, from the st.com web site, which was delivered a few weeks ago.