cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L05 + SPI not work after stop mode

SMila
Associate

Hi,

I am trying to use an e-paper and a STM32L053C8 microcontroller.

When i use the display in the first cicle, all works fine, but after wake up from stop mode, the display not works. Maybe the SPI interface not start well or i am doing somthing wrong.

This is my first days with this microcontroller and hal programming structure.

Thanks,

Regards,

This is my inicialization code:

/**

 * @brief SPI1 Initialization Function

 * @param None

 * @retval None

 */

static void MX_SPI1_Init(void)

{

 /* USER CODE BEGIN SPI1_Init 0 */

 /* USER CODE END SPI1_Init 0 */

 /* USER CODE BEGIN SPI1_Init 1 */

 /* USER CODE END SPI1_Init 1 */

 /* SPI1 parameter configuration*/

 hspi1.Instance = SPI1;

 hspi1.Init.Mode = SPI_MODE_MASTER;

 hspi1.Init.Direction = SPI_DIRECTION_1LINE;

 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

 hspi1.Init.NSS = SPI_NSS_SOFT;

 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;

 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

 hspi1.Init.CRCPolynomial = 7;

 if (HAL_SPI_Init(&hspi1) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN SPI1_Init 2 */

 /* USER CODE END SPI1_Init 2 */

}

This is the code to entry in stop mode and the next code lines that they are executed:

/* Enter Stop Mode */

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

HAL_UART_Transmit(&hlpuart1, (uint8_t*)"Sleep mode activated...\r\n", sizeof("Sleep mode activated...\r\n"), 20);

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

/* Configures system clock after wake-up from STOP: enable HSE, PLL and select

PLL as system clock source (HSE and PLL are disabled in STOP mode) */

//HAL_Init();

SystemClock_Config();

MX_GPIO_Init();

MX_ADC_Init();

MX_LPUART1_UART_Init();

MX_USART2_UART_Init();

MX_RTC_Init();

MX_SPI1_Init();

MX_TIM2_Init();

HAL_UART_Transmit(&hlpuart1, (uint8_t*)"Wake-Up...\r\n", sizeof("Wake-Up...\r\n"), 20);

0 REPLIES 0