cancel
Showing results for 
Search instead for 
Did you mean: 

How to test STM32F469AI of packaging type WLCSP168 if its receiving power?

Chandu
Associate II

Hi everyone,

I have the STEVAL-IDP005V1 sensor board on which STM32F469AI MCU is present. I suspect that something is wrong with the D9 pin of MCU which is supposed to receive 3.3V from the power management unit on the board which I tested to be up and fine. However the packaging type of the MCU does not expose any pins to be used for debugging and there are no coupling capacitors to that pin (from schematic).

So how can I test that pin without damaging the MCU?

Thanks in advance

-Chandrasekhar DVS

0690X000009Z2FAQA0.png

0 REPLIES 0