cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH datasheet - STATUS_REG_AUX description is wrong / unhelpful

Andrew Neil
Evangelist

Latest datasheet: DocID17530 Rev 2, December 2016, page 33:

0690X000009YvDLQA0.png

https://www.st.com/resource/en/datasheet/lis3dh.pdf

Looks like a copy-and-paste error: all the references to "axis" should say "ADC" ?

Also, there is no description of the operation of this register in relation to the ADCs.

In fact, it isn't even specifically stated that this does relate to the ADCs!

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @Andrew Neil​ , please consider the block diagram below: the ADCs are inputs of the device, so they can substitute the MEMS in generating the data output for the 3 axis. So, in the hypothesis that the 3 ADCs are fed and working, the STATUS_REG_AUX detects when an overrun occurs in one of the 3 ADCs, that refers each one to one axis. Are you using the ADCs for a particular reason? Regards

0690X000009YvXzQAK.png

I think you missed my point!

The point is that the text in the descriptions should say "ADC1", "ADC2", "ADC3" - not "Axis 1", "Axis 2" and "Axis 3".

The use of the word "Axis" is confusing & misleading.

Especially since the ADC Data registers do say "ADC1", "ADC2", "ADC3" !