cancel
Showing results for 
Search instead for 
Did you mean: 

How connected the physical buffer of the STM32L4R9 discovery board on the external PSRAM (with or without using GFXMMU)?

DMart.19
Associate

Hello! Has anyone ever already connected the physical buffer of the STM32L4R9 discovery board on the external PSRAM (with or without using GFXMMU)? All STM32 Cube examples are using a buffer in internal RAM...

When I put the buffer in PSRAM, the rendering on LCD is wrong: some white lines appear and sometimes all the content is wrong.

Actually, I have some LTDC FIFO underrun interrupts. I have follow advices of application note DM00287603.pdf (chapter LTDC required bandwidth) without success. :(

1 REPLY 1
STrop
Associate II

Hello David,

I currently try to do the same without satisfaction.

Did you manage to put the physical area of GFXMMU to PSRAM ?

Thanks

Simon