cancel
Showing results for 
Search instead for 
Did you mean: 

Motor control Workbench is generating code with errors

NK.13
Associate II

i am using STEVAL-SPIN3201 development board for the project.first i start the workbench and give the board details then after setting i give to generate code.the workbench is giving the code with errors.why this happens...?

i am attaching my log which is generated from workbench..

3 REPLIES 3
NK.13
Associate II

i have generated code from motor control workbench and when i build this code the error came as,

region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ Problem

StSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_24_07 C/C++ Problem

i tried for optimised the code code then the there is no error but motor is not working well........

please help...

Ozone
Lead

Try to keep it in one tread...

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards