2019-07-12 07:01 AM
Hello,
I'm confused about the capability of STM32H753 to operate at a CPU frequency of 480MHz.
The datasheet mentions that 480MHz is the max CPU clock frequency under VOS0, and the reference manual describes how to activate voltage scaling to VOS0.
However I've read on a developpers' forum that 480MHz is supported only on some revisions of this product.
Do you have feedback on this issue ?
Thank you
2019-07-12 07:14 AM
Did you have a look at the most recent datasheet? Speed is dependant on Chip revision and specs for the different revisions are given in the datasheet.
2019-07-12 07:21 AM
Thank you, I got it. Does that mean that the VOS0 mode is just not available on rev Y ?
2019-07-12 08:22 AM
Look in a recent reference manual to find out.
2019-07-12 08:56 AM
2019-07-12 09:24 AM
The datasheet specs are also valid at the corners like low voltage and high temperature. So you can expect to be able to overclock in a more friendly environment.
2019-07-12 09:52 AM
I'd imagine so, my point more generally would be a design with 120 MHz of head-room, and no immediately obvious critical-path issues has quite a lot of leeway to operated beyond 400 MHz
ATMEL's first generation CM7 design, with an FPU-D I might add, shipped supporting 300 MHz 2015Q2 as I recall
F7 uses a 90 nm process, the H7 uses a 40 nm process.
2019-07-15 11:20 PM
Well that's the point, the reference manual details the usage of VOS0 but does not mention limitations on a given revision (which makes sense). And the datasheet for rev Y simply does not mention characteristics for VOS0.
2019-07-15 11:22 PM
Thank you for the details. I'm working in a critical environment with many norms and certifications to respect, so unfortunately I cannot go beyond what the manufacturer guarantees.