cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

garyng98
Associate

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

Dear all, I am new to STEVAL-BCN002V1.

I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V1.

As I will only use acclerometer and pressure sensor to get free-fall function, step counter, acitivites recongition.

Also, I will like to ask why am I able to add the customised C code which I had build using algobuilder to the whole project.

Please teach.

Best Regards

Gary

1 REPLY 1
Eleon BORLINI
ST Employee

​Hi @garyng98​ , please consider that the STEVAL-BCN002V1 is based on the X-CUBE-MEMS1 firmware library package. To be more specific, the mid-level code function explanation can be found in the proper User manuals, such as:

Regards