cancel
Showing results for 
Search instead for 
Did you mean: 

What in-circuit debugger/programmer should I use for STEVAL-MKSBOX1V1?

Eugene Agustin
Associate II

I am using STEVAL-MKSBOX1V1 and I want to do some changes in the firmware.

What in-circuit debugger/programmer should I use? Should I use ST-LINK/V2 or STLINK-V3SET or STLINK-V3MINI?

Please help me. Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @Eugene Agustin​ , if programming through JTAG/serial wire debugging (SWD), I suggest you to use the ST-LINK/V2 programmer because of 1.8V level compatibility with ,ow power STM32L4R9. The HW connection is the connector numbered "8". Board schematic will be available soon on st.com. Regards

View solution in original post

27 REPLIES 27

Manual says "The board includes the ST-LINK V3 (with UART pins for debugging) compatibility."

Unfortunately no pictures of the back side of the board.

Suggest you contact your local sales office and discuss.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Eugene Agustin
Associate II

Here is the back side of the board.

Please look at the attached image thank you

No picture attached. Make sure you upload and insert it.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Eugene Agustin
Associate II

0690X000009YY8cQAG.png

Sorry I forgot to insert.

Thank you

Eleon BORLINI
ST Employee

Hi @Eugene Agustin​ , if programming through JTAG/serial wire debugging (SWD), I suggest you to use the ST-LINK/V2 programmer because of 1.8V level compatibility with ,ow power STM32L4R9. The HW connection is the connector numbered "8". Board schematic will be available soon on st.com. Regards

Hi @Eleon BORLINI​ ,

I already bought an ST-LINK/V3 since it is the newer version. Am I right that it will work on SensorTile.box for programming?

Thank you

DIM
Associate II

Hi @Eugene Agustin​ did you find an answer to your question?

I know the STLINK-V3SET is compatible with the MKSBOX1V1 as per this post.

This document compares STLINK-V3SET and STLINK-V3MINI on Page 2.

Hi @DIM​ 

Not yet.

Thank you for sharing the information. I need some quick start guide or manual on how to use STLINK-V3SET on MKSBOX1V1.