cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with trueSTUDIO v9.3.0 not with trueSTUDIO v7.1.0

Skira.17
Associate II

I have created a project in trueSTUDIO v7.1.0 on computer 1 and compiled it well without any errors. But when I imported the same project to trueSTUDIO v9.3.0 on computer 2 it is giving me an error.(ERROR: Program "GCC" not found in PATH ).

When I checked the PATH variable in (Properties-> C/C++ Build->Environment(PATH: C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.3.0\ARMTools\bin; )) .Its was fine as bin contains the arm-atollic-eabi-gcc compiler. What might be the problem? Did anyone faced the same issue? Any help will be appreciated. Thank you.😁

1 REPLY 1
Malachi
Associate II

This was biting me too. Read PREVENT “GCC NOT FOUND IN PATH�? ERROR section under

https://usermanual.wiki/Document/AtollicTrueSTUDIOforSTM32UserGuide.1420695683/help

It helped me