2019-06-21 12:23 AM
Just got my STM32H745 DISCO today. I notice ST uses ST-Link V3 on all dual core boards. Does ST-Link V2 still work for dual core lines? I searched around on ST website and could not find any answers. Beers provided for anyone giving a hint 😉
Solved! Go to Solution.
2019-06-26 06:32 AM
Back to the original question: "Does ST-Link V2 still work for dual core lines? " Replace "still" by "with recent firmware" and the answer is yes.
2019-06-21 12:35 AM
Not sure. The V3 is definitely faster, and can individually talk to each core based on the newer SWD protocol. Would need to double check if the V2 allows for this in the STM32 Cube Programmer with newer firmware.
I do know you have to be aware of the higher clocking rate when computing the SWV baud rate. In one of the test systems the clock was 15 MHz rather than 2 MHz.
2019-06-21 12:40 AM
2019-06-21 12:52 AM
Thanks Clive. V3 does perform a lot better on my test run. Problem is it is implemented with an F7 chip, which is like costing a fortune in some case. I hope the granny F1 v2 still work like you said, at least for the CM7. I just ordered converter and cable to give it a try. Any more inputs on the subject will be very welcomed.
2019-06-24 09:46 PM
Alright, got my tag-connect cable today and use a standalone ST-Link V2 to debug H745 Disco. It does show two cores. V2 works! Just much slower. Anyway, I am happy.
2019-06-25 01:24 AM
The M7 in the H745 has controll over the M4, In the H7 Disco application, the M4 is only visible when the EMBC application is running.
2019-06-26 06:04 AM
AC6 wins(!).
Atollic and CubeIDE prevented me from using my H745-DISCO, I don't have IAR, and I couldn't find enough pieces to do it all in bare Eclipse, but I tried sw4stm32 v2.9 and I was blinking LEDs (both cores) in two hours.
It does dual-core build, ST-Link/V3 (DISCO native) and dual-core debug. Even openOCD runs with no fiddling. Apparently AC6 has had this since April.
2019-06-26 06:32 AM
Back to the original question: "Does ST-Link V2 still work for dual core lines? " Replace "still" by "with recent firmware" and the answer is yes.