cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_SAI_FlushRxFifo function implementation

raffin
Associate III

On the UM1725, DocID025834 Rev 5, par 57.2.1, pag. 766 A function called HAL_SAI_FlushRxFifo() is contemplated among the "SAI HAL driver additional function list".

On the hal driver, this function is declared on the comments but it is not implemented.

Is there an implementation available?

I have a huge delay on the Rx which disappears, while debugging, if I put a breakpoint on the audio task and then restart it.

Thank you in advance.

0 REPLIES 0