cancel
Showing results for 
Search instead for 
Did you mean: 

When I generate the IAR V7 code by STM32CubeMX5.2.1 and TM32CubeF4 Firmware Package V1.24.1,Two errors occurred.

�?�
Associate

Hello,

When I generate the IAR V7 code by STM32CubeMX5.2.1 and TM32CubeF4 Firmware Package V1.24.1,Two errors occurred. 

The first,Fatal Error[Pe035]: #error directive: intrinsics.h is already included previously! E:\AC_Project\AC_Project0506\Drivers\CMSIS\Include\cmsis_iccarm.h 483 。

The second,the IAR V7 can not recognizable “__restrict�? 

#ifndef __RESTRICT

#define __RESTRICT __restrict

#endif 

Looking forward to your help,Thank you.

0 REPLIES 0