cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo_F429ZI Ethernet echo example

justin11
Associate III

Hi,

I'm new to STM and finding the mash-up of tools and examples quite frustrating.

I purchased a Nucleo_F429ZI with Ethernet and there only seems to be one Ethernet example in the driver repository "LwIP_HTTP_Server_Netconn_RTOS". We wanted to use the TCP Echo client without RTOS, but that seems to be missing.

Also none of the examples seem to be geared around there own STM32CubeIDE ?

Can anyone help ? I would like to be able to use the CubeMX tool for chip setup and have a working example of the TCP Echo client without RTOS, so i can use as a platform to develop off of.

Should I move away from the STM32CubeIDE ?

any help would be much appreciated....

2 REPLIES 2
Geraldo Pereira
Associate II

Hi Justin,

Did you solve your problem? I´m with the same problem.

Do you suggest other board that have support to ethernet socket?

Thanks,

Geraldo.

Cartu38 OpenDev
Lead II

Have you got a try to STM32Cube_FW_F4_V1.25.1\Projects\STM32F429ZI-Nucleo\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS ?

Ok SW4STM32 based example but such is fully STM32CubeIDE supported. Just rely on proper import feature and you're done:

0693W000004KQ9oQAG.png