2019-06-10 01:05 PM
2019-06-10 01:14 PM
2019-06-10 03:16 PM
What are your actual 'required capabilities' ? I assume if you needed all of them, you would use the ADI chip
2019-06-10 03:21 PM
Floating point operations
16 bit ADC *2
UART support RS-485
Ethernet support
2 DAC 12 Bit
Cache Memory - 128 -348K byte
Flash Memory – 2 * 10^6 * 8 bits
Clock Speed is 240 MHz
Low, high pass filtering available
Watchdog
SPI and I2C Communication Possible.
DMA
MPU
These all I need
2019-06-10 03:24 PM
Some of the high end processors can do most of that, but the ADC will always be the gotcha. ADI's ones are simply better.
Load up the MCU finder and enter what you really need
2019-06-10 04:39 PM
2019-06-10 08:32 PM
They have stopped the support (Very limited Support available) for the ADSP - CM408F (Or any of the DSP parts which they have produced).
My major concern here is ADCs which they have used in their parts, according to @MikeDB if they are one of the best then I have no other option to go with AD parts
2019-06-11 01:09 AM
Or you could use an STM part and an external ADC ? Some STM MCUs have 16 bit resolution but the accuracy and linearity are woeful, and more importantly very batch dependent so you can't just calibrate it out at design time.
And I certainly hope ADI aren't reducing support for their main DSPs - there are whole industries built around SHARC and Blackfin.
Mind you, this is the company that obsoleted the industry-standard microphone amp IC back in 1999 !
2019-06-11 08:49 AM
I do not want to compromise on ADCs and Yes they have limited the support on DSPs.
2019-06-11 08:52 AM
I'd go for an F7 part with the bits you need and an SPI A-D convertor chip then