cancel
Showing results for 
Search instead for 
Did you mean: 

Is VCP diver able to handle several devices on Windows 10?

JLojo
Associate III

Hello,

I'm using VCP to communicate with an STM32F303 device, which works well.

However, when I plug a second device on the same computer, it fails to enumerate properly with the message 'This device cannot start. (Code 10)'.

Is that a known issue?

Is there a way to connect several STM32 on the same computer?

Thanks

jyl

4 REPLIES 4

And if you unplug the first device and plug in the second one?

Don't they draw excessive power?

JW

Pavel A.
Evangelist III

Non unique "serial number" ?

-- pa

JLojo
Associate III

Hmm, maybe same ID...

I thought serial number was assigned automatically for each device...

I'll check this in mode details.

Thanks Pavel!

Both work perfectly as long as they are alone on the computer...

jyl